This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Standalone program to flash Piccolo without IDE?

Other Parts Discussed in Thread: UNIFLASH

I need to be able to re-flash our Piccolo-based board out in the field during testing, as this device is placed in an embedded vehicle detection system.  The test guy just has his laptop, and I'd rather not cough up for another full license just to re-flash a board...

All help appreciated!

Ed Averill

  • Hi Ed,

    Edward Averill said:

    I need to be able to re-flash our Piccolo-based board out in the field during testing, as this device is placed in an embedded vehicle detection system.  The test guy just has his laptop, and I'd rather not cough up for another full license just to re-flash a board...

    All help appreciated!

    You can use CCS Uniflash or C2Prog. Both are standalone programming applications for C2000 devices.

    Just google and give them a try. Short list the one you feel the service guy would be comfortable with.

    Regards,

    Gautam

  • Excellent, thanks a lot! I see it does MSP430s as well, which is great as we'll have the same issue with field testing our MSP430 product.

    Have a great rest of the week!

    Ed Averill

  • That's Great! You got the tool you were looking for.

    Goodluck & Regards,

    Gautam