Hello all,
I am trying to run the flash_f28035 example on TMSDOCK28035 experimenters kit. If it is successful, I should see GPIO34 toggle right?
This is what I did, please tell me what I am missing.
I added FLASH symbol in properties of the project. After I built the project, I debug, and I can see two pop up windows, saying erasing flash sectors and loading program. I then disconnect JTAG USB cable, reset the power on the experimenter's kit and nothing happens. I dont see GPIO34 toggle.
pretty new to FLASH, although i have been running my custom board with success on RAM. Please help!
-Sandhya