Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301, MOTORWARE
Hey Chris,
I am a new user to the DRV8301-69M-KIT. I seem to be facing some problems while using the InstaSPIN-FOC GUI. I purchased an AC SERVO Motor from Panasonic to implement FOC for my research. The problem that I am facing is that every time I try to start the automatic identification algorithm on the InstaSPIN-FOC, the stator inductance value turn out to be very abnormal like (5e-10 H) both for d and q axis.
I am using a 24 volts power supply.I used the default identification parameters after which I tried to manipulate the Res Current and the Ind Current to 20% of the rated value, even then the inductance value was negligible. Is there something I am doing wrong here?
Following are my motor parameters.
3 phase AC 43V @ 50W. Rated frequency is 200 Hz. Rated Speed is 3000rev/min. Rated/Max Current: 1.1A/4.7A
Motor Pole pairs = 4