Other Parts Discussed in Thread: TMS320F28027, MOTORWARE
Hi,
I have boght TI C2000 launchpad from ebay, arrived and seems to work
But when I got the DRV8301 I got error while trying to RUN it, here in forum I was told that the errors might be becuase I didn't connect DRV8301 - but when got it had same errors.
Now when I got another TI C2000 - it is working ok with it!
So my question as before - do I need something special that is burned when I get this board from factory? (because the code inside looks different - I see by LEDS)
And when I can download the BASIC first code that arrives with new board?
Can I read the code (hex file to my computer) - and rewrite it to the second board ??
I was told that any way motorware download RAM on the run (and I see it taking some .out file while running)
Thanks for any help
Roee
I was told that I can find the answer here ?
Is the difference between 2 C2000 boards is code only ?
Can I burn the code for the SPIN ?
Thanks,
Roee