Other Parts Discussed in Thread: CONTROLSUITE, INSTASPIN-BLDC
Hello, everyone =)
I have a question about DRV-8301-H2-C1 kit.
I got this one to play with a motor and to build a control system. It's told to use Insta-SPIN BLDC app for this kit (it's told so on TI.com). But it's all is hidden inside a library.
I know, that there's Insta-SPIN FOC and MOTION with source files, and I have them in ControlSUITE. But they are for 2802x, 2805x, 2806x.
And i have 28035 Piccolo controlCard. I have also a Concerto ControlCARD.
SO, the question is: where can I get Source projects of InstaSPIN-BLDC library? If it's not possible, can I use 28035 + IS-FOC on this board?
Thank you =)
P.S.: it's told, that "Piccolo CCs are completely interchangeble". So I guess, F28027 project should work well on F28035, cuz latest is even more... powerful. I also think, that my Kit won't mind if I use another microcontroller. But I'd like to be sure =)