Other Parts Discussed in Thread: ISO1050, CONTROLSUITE, ISO1050EVM
Hi
I am not able to get toggling output at TXD pin of CAN.The code is attached below for F28335.Kindly Help me out..
Is the program correct? Can someone please help out.
CAN-Rx
//
// Lab CAN_2 : TMS320F2812
// (C) Frank Bormann
//
//###########################################################################
//
// FILE: Lab_CAN_2.c
//
// TITLE: DSP28 CAN - Receive with the Zwickau-adapterboard
//
// Extended CAN-Frame is received with 1 MBPS
// from highspeed-CAN
// Jumper JP4 : 2-3 ( 120 Ohm enabled)
// Jumper JP5 : 1-2 ; Jumper JP6 _ 1-2 ( highspeed transceiver SN
//
// Aim of the test :
// Receive a 1 byte dataframe with Identifier 0x10000000
// and show the databyte on the LED's at GPIO-Port B7...B0
// Mailbox 1 is used as receiver
// Identifier : 0x1000 0000
// DLC = 1
//
// Frequency Osscillator : 30MHz
// PLLCR = 0xA : multiply by 5
// SYSCLKOUT = CLKIN = 150MHz
// Highspeed - Prescaler (HISPCP = 0x0001; div by 2 ) : 75 Mhz
// Lowspeed - Prescaler (LOSPCP = 0x0002; div by 4 ) : 37.5 Mhz
//###########################################################################
//
// Ver | dd mmm yyyy | Who | Description of changes
// =====|=============|======|===============================================
// 1.0 | 09 May 2003 | F.B. | Startup Version for Lab_CAN_2
// 2.0 | 27 Nov 2003 | F.B. | adapted to header-files Version 1.00
//###########################################################################
// CAUTION : DSP281x_ECan.h , Version 1.0 ( Hareesh) contains an error
// the byte field of struct CANMDL_BYTES and CANMDH_BYTES
// have the wrong order ( Byte1 to 4)instead of Byte 4 to 1)
// MODIFY : inside DSP281x_ECan.h modify the two structures to :
// struct CANMDL_BYTES { // bits description
// Uint16 BYTE3:8; // 31:24
// Uint16 BYTE2:8; // 23:16
// Uint16 BYTE1:8; // 15:8
// Uint16 BYTE0:8; // 7:0
// };
//
// struct CANMDH_BYTES { // bits description
// Uint16 BYTE7:8; // 63:56
// Uint16 BYTE6:8; // 55:48
// Uint16 BYTE5:8; // 47:40
// Uint16 BYTE4:8; // 39:32
// };
//##########################################################################
#include "DSP28x_Project.h"
#define IDENTIFIER 0x10000000
// Prototype statements for functions found within this file.
void Gpio_select(void);
// Global Variables
/* Create a shadow register structure for the CAN control registers. This is
needed, since, only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents. This is
especially true while writing to a bit (or group of bits) among bits 16 - 31 */
struct ECAN_REGS ECanaShadow;
main()
{
// Initialize System Control registers, PLL, WatchDog, Clocks to default state:
// This function is found in the DSP28_SysCtrl.c file.
InitSysCtrl();
// Initialise the physical pins of the DSP
Gpio_select();
/* Initialize the CAN module */
InitECan();
/* Write to the MSGID field - MBX number is written as its MSGID */
ECanaMboxes.MBOX1.MSGID.all = IDENTIFIER; // extended identifier
ECanaMboxes.MBOX1.MSGID.bit.IDE = 1;
/* Configure Mailbox 1 as Receiver mailbox */
ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
ECanaShadow.CANMD.bit.MD1 = 1;
ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
/* Enable Mailbox 1 */
ECanaShadow.CANME.all = ECanaRegs.CANME.all;
ECanaShadow.CANME.bit.ME1 = 1;
ECanaRegs.CANME.all = ECanaShadow.CANME.all;
/* Begin Receiving */
while(1)
{
do {
ECanaShadow.CANRMP.all = ECanaRegs.CANRMP.all;
}
while(ECanaShadow.CANRMP.bit.RMP1 != 1 ); // Wait for RMP1 to be set..
ECanaShadow.CANRMP.bit.RMP1 = 1;
ECanaRegs.CANRMP.all = ECanaShadow.CANRMP.all; // Clear RMP1 bit and start again
}
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all=0; //PORT A IS THE can PORT
GpioCtrlRegs.GPAMUX2.all=0;
GpioCtrlRegs.GPBMUX1.all=0;
GpioCtrlRegs.GPBMUX2.all=0;
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 3; // setting gpio19 as CANTXA
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; // setting gpio18 as CANRXA
GpioCtrlRegs.GPADIR.all=0; // GPIO PORTs as input
GpioCtrlRegs.GPBDIR.all=0x00ff; // GPIO Port B15-B8 input , B7-B0 output
GpioCtrlRegs.GPCDIR.all=0;
GpioCtrlRegs.GPAQSEL1.all=0; // Set GPIO input qualifier values
GpioCtrlRegs.GPAQSEL2.all=0;
GpioCtrlRegs.GPBQSEL1.all=0;
GpioCtrlRegs.GPBQSEL2.all=0;
GpioDataRegs.GPBDAT.all = 0x0000; // Switch off LED's ( B7...B0)
EDIS;
}
CAN-Tx
//
// Lab CAN_1 : TMS320F2812
// (C) Frank Bormann
//
//###########################################################################
//
// FILE: Lab_CAN_1.c
//
// TITLE: DSP28 CAN - Transmission with the Zwickau-adapterboard
//
// Jumper JP4 : 2-3 ( 120 Ohm enabled)
// Jumper JP5 : 1-2 ; Jumper JP6 _ 1-2 ( highspeed transceiver SN
//
// Aim of the test :
// Transmit the status of the 8 switches from GPIO - Port B15...B8
// repeat the transmission every second
// Mailbox 5 is used for transmission
// Identifier : 0x1000 0000
// DLC = 1
//
// Frequency Osscillator : 30MHz
// PLLCR = 0xA : multiply by 5
// SYSCLKOUT = CLKIN = 150MHz
// Highspeed - Prescaler (HISPCP = 0x0001; div by 2 ) : 75 Mhz
// Lowspeed - Prescaler (LOSPCP = 0x0002; div by 4 ) : 37.5 Mhz
//###########################################################################
//
// Ver | dd mmm yyyy | Who | Description of changes
// =====|=============|======|===============================================
// 1.0 | 09 May 2003 | F.B. | Startup Version for Lab_CAN_1
// 2.0 | 27 Nov 2003 | F.B. | adapted to header-files Version 1.00
// | | |
//###########################################################################
// CAUTION : DSP281x_ECan.h , Version 1.0 ( Hareesh) contains an error
// the byte field of struct CANMDL_BYTES and CANMDH_BYTES
// have the wrong order ( Byte1 to 4)instead of Byte 4 to 1)
// MODIFY : inside DSP281x_ECan.h modify the two structures to :
// struct CANMDL_BYTES { // bits description
// Uint16 BYTE3:8; // 31:24
// Uint16 BYTE2:8; // 23:16
// Uint16 BYTE1:8; // 15:8
// Uint16 BYTE0:8; // 7:0
// };
//
// struct CANMDH_BYTES { // bits description
// Uint16 BYTE7:8; // 63:56
// Uint16 BYTE6:8; // 55:48
// Uint16 BYTE5:8; // 47:40
// Uint16 BYTE4:8; // 39:32
// };
//##########################################################################
#include "DSP28x_Project.h"
#define IDENTIFIER 0x10000000
// Prototype statements for functions found within this file.
void Gpio_select(void);
void delay_loop();
Uint16 loopcount =0;
// Global Variables
/* Create a shadow register structure for the CAN control registers. This is
needed, since, only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents. This is
especially true while writing to a bit (or group of bits) among bits 16 - 31 */
struct ECAN_REGS ECanaShadow;
main()
{
// Initialize System Control registers, PLL, WatchDog, Clocks to default state:
// This function is found in the DSP28_SysCtrl.c file.
InitSysCtrl();
// Initialise the physical pins of the DSP
Gpio_select();
/* Initialize the CAN module */
InitECan();
/* Write to the MSGID field */
ECanaMboxes.MBOX5.MSGID.all = IDENTIFIER;
ECanaMboxes.MBOX5.MSGID.bit.IDE = 1; // Extended Identifier
/* Configure Mailbox under test as a Transmit mailbox */
ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
ECanaShadow.CANMD.bit.MD5 = 0;
ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
/* Enable Mailbox under test */
ECanaShadow.CANME.all = ECanaRegs.CANME.all;
ECanaShadow.CANME.bit.ME5 = 1;
ECanaRegs.CANME.all = ECanaShadow.CANME.all;
/* Write to DLC field in Master Control reg */
ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 1;
ECanaMboxes.MBOX5.MDL.all = 0x00000005;
ECanaMboxes.MBOX5.MDH.all = 0x00000005;
/* Begin transmitting */
for(;;)
{
ECanaShadow.CANTRS.all = 0;
ECanaShadow.CANTRS.bit.TRS5 = 1; // Set TRS for mailbox under test
ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all;
do
{
ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
} while(ECanaShadow.CANTA.bit.TA5 == 0 ); // Wait for TA5 bit to be set..
ECanaShadow.CANTA.all = 0;
ECanaShadow.CANTA.bit.TA5 = 1; // Clear TA5
ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;
loopcount ++;
}
asm(" ESTOP0"); // Stop here
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all=0; //PORT A IS THE can PORT
GpioCtrlRegs.GPAMUX2.all=0;
GpioCtrlRegs.GPBMUX1.all=0;
GpioCtrlRegs.GPBMUX2.all=0;
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 3; // setting gpio19 as CANTXA
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; // setting gpio18 as CANRXA
GpioCtrlRegs.GPADIR.all=0; // GPIO PORTs as input
GpioCtrlRegs.GPBDIR.all=0x00ff; // GPIO Port B15-B8 input , B7-B0 output
GpioCtrlRegs.GPCDIR.all=0;
GpioCtrlRegs.GPAQSEL1.all=0; // Set GPIO input qualifier values
GpioCtrlRegs.GPAQSEL2.all=0;
GpioCtrlRegs.GPBQSEL1.all=0;
GpioCtrlRegs.GPBQSEL2.all=0;
GpioDataRegs.GPBDAT.all = 0x0000; // Switch off LED's ( B7...B0)
EDIS;
}
void delay_loop()
{
long i;
for (i = 0; i < 10000000; i++) {}
}