Good day,
In the Intermediate GUI there is an option for the G3 firmware of the TMDSPLCKIT-V3, which are called "Level" and "Mask".
1. "Level" definitely I do not get what it does. In the documentation of TI the description for it says only: "From 0 to 32, with 32 the maximum".
2. "Mask" I understand allows selecting some of the sub-carriers. It would have sense with the options CENELEC A 36 and CENELEC A 25, since I understand G3 works in the CENELEC A band exclusively. Nevertheless I do not understand the options CENELEC B, BC and BCD.
3. Why it is said that G3 is more flexible than PRIME regarding the frequency. I see that G3 is also fixed to the CENELEC A band.
Thank you for the help!!!
Sincerely,
Diego Ballen Cantor