Other Parts Discussed in Thread: CONTROLSUITE
Hi,
Apologies if this has been covered before, I cannot find anything in the Forums...
I have a Docking Station USB-EMU [R3] with an F2808 ControlCARD fitted.
I've used ControlSUITE and taken the SCI-Echoback example from the F2807 Code Examples and ported it to the F2808 device. I can successfully transmit a message from the F2808 to PC (RealTerm), however, when I try to send a message back from RealTerm to the F2808 I do not receive it.
I've been through the registers several times, checking the various settings and I cannot see anything wrong from the Software point of view. I loaded the sci_loopback_interrupts Code Example and this works fine (I'm aware it's not communicating with the PC).
The FTDI chip is ok, I'e checked the configuration with FT_Prog.
I suspect the problem is in the USB - UART bridge and the signal isn't reaching the Processor. After a bit of searching I found that R18 on the ControlCARD has to be 0ohm (which it is) and that J9 on the docking station has to be jumpered (which it is now). I still cannot receive any data from RealTerm.
Tomorrow I will connect the scope to try and establish what is happening but I thought I would ask here in case there is an easy/quick solution that I've missed.
Or another alternative, does anyone have any working code for the F2808 that allows UART comms on the Docking Station?
Any assistance appreciated.
Mike.