Other Parts Discussed in Thread: CONTROLSUITE
Has anyone been able to get the Spectrum Digital XDS510USB emulator to work with the controlCARD Docking Station(R4.1)?
I have connected the JTAG to the 14-pin header on the controlCARD.
I still get the following error:
IcePick_C_0: Error connecting to the target: Error 0x80000244/-2131 Fatal Error during: Register, Initialization, OCS, Cannot access register at 0x00000030
I changed the target configuration file to select the XDS510USB Emulator and chose the correct device.
Is there anything else I need to do? I am using CCS v6.0.0.00190 and have a Release 4.1 of the controlCARD.