Other Parts Discussed in Thread: MOTORWARE, BOOSTXL-DRV8301, DRV8301, DRV8312, INSTASPINUNIVERSALGUI
This is the third time I am posting on TI Forums and for some random reason by post always gets deleted.
Anyways, I am a new user to the DRV8301-69M-KIT. I seem to be facing some problems while using the InstaSPIN-FOC GUI. I purchased an AC SERVO Motor from Panasonic to implement FOC for my research. The problem that I am facing is that every time I try to start the automatic identification algorithm on the InstaSPIN-FOC, the stator inductance value turns out to be very abnormal like (5e-10 H). I tried reading other posts on InstaSPIN motor solutions and I figured that the GUI won't do much in low inductance motor identification since the SW poles are fixed and cannot be changed after which I turned to motorware projects. I tried changing the user.h parameters but of no use. I cannot get my motor up to speed and everytime I go beyond 200 RPM, it starts buzzing and vibrating or at times, turning in the opposite direction.
I am using a 24 volts bus but I have a variable power supply. I tried to satisfy the condition (USER_IQ_FULL_SCALE_FREQ_Hz < 4 * USER_VOLTAGE_FILTER_POLE_Hz). Can anyone tell me if there is there something I am doing wrong here?
Following are my motor parameters.
3 phase AC 43V @ 50W. Rated frequency is 200 Hz. Rated Speed is 3000rev/min. Rated/Max Current: 1.1A/4.7A
Motor Pole pairs = 4
I am attaching the user.h file for reference.
Regards,
Fahad Raza