This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash programming problem

Hi,

I'm using f28335 ezdsp programming it with matlab r2010b and ccs v3.3

the problem is when i reach final step in programming it after i hit excute operations in ccs i have this error

Flash API Error #65535:
The device is in limp mode

I don't figure the problem.

  • Hi Kevin,

    It sounds like the input clock is not properly connected to the device.

    Please check the input clock to the DSP. Also, check XCLKOUT pin to ensure device is not in limp mode. SYSCLKOUT frequency in limp mode could be from 1 - 5 MHz.

    Regards,

    Gautam