Other Parts Discussed in Thread: F28M36H33B2
Hi,
In new design we are planning on using the F28M36H33B2ZWTT, we have a question regarding the PWM pin mapping.
We want to use the ePWM9A/B and ePWM10A/B on pins K2(PS0),L3(PS1),L2(PS2) and M3(PS3).
Can we use this the same way as ePWMA1A/B on pins D1(PA0)E3(PA1)?
We have a development board but these pins are not routed to measurable outputs as far as we know. (F28M36x (180pin) cCARD)
The datasheet (f28m36h33b2.pdf, feb 2014) is a bit contradictory on this point, in Table 4-48 it is mentioned that they can be used as stated above. However it is unknown whether it can be used according Table 4-59, in this table PERx is mentioned in. Where does this PER stand for?
Thanks in advance!