Hi all,
We are using c2prog to download the HEX file on SCI port in the boot mode for TMS320F28335.
In the tool different options are given to select the frequency of the processor.
We placed 24MHz oscillator on our board and trying to dump the code through SCI interface in boot mode, it is not working.
When we replaced 24MHz with 30MHz oscillator, then the code is dumped into the TMS320F28335.
Could anybody please help us on this issue.
We want to use 24MHz oscillator on our boards.
Thankyou,
Lakshmi.