Other Parts Discussed in Thread: DRV8302, DRV8301, DRV8303, MOTORWARE, INSTASPINUNIVERSALGUI
Hi,
first of all I'm new to that motor control stuff. We have to develop a FOC motor control solution so I'm looking where to start. I think I will get myself the Launchpad XL + the DRV8301-Booster Board to get in first touch with the topic.
May I still ask you some question before starting?
- Which DRV83xx device should I chose for a new design? I understood that the difference between DRV8301 and DRV8302 is the changed SPI-IF but with DRV8303 it's back? Shall I stick with the DRV8303 if in doubt? I can't see any difference beside the IF!?
- Is it possible to change the motor control parameters later on per protocol (SPI/UART/..)?
- Is it still possible to run the Motorware GUI with one's own board? If yes: Is there anything special needed (i.e. some emulator?) or does it work out of the box via JTAG, just like the Eval-Board?
Thanks for your support in advance!
Kind regards,
Stephan