Hello,
When we use a docking station to program a F28335 control card, everything works fine. But when we try to program the F28335 chip on a hardware, we keep getting this error:
C28xx: Error: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? (Emulation package 5.1.232.0)
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx: GEL: File:
We supplied the docking station 5V and programmed it via JTAG. The current was around 0.20A. But when we try the same on hardware, we gave 3.3V and the current was around 0.10A. We have removed the MAX3221ECPW part of the control card since we dont need the TX-ISO and RX-ISO. Could you please let us know where we are going wrong?