Other Parts Discussed in Thread: TMS320F28069
Hi,
I have two VSI in parallel connection, they share the dc-link. Each of them is controlled by a TMS320F28069 control card. I haven't implemented the PWM synchronization. I have three-phase RL load to each VSI. When I measure the A-phase curents for both VSI outputs, the strange thing is that, their phase shift is always changing. Since I dont have PWM synchronization, for sure there should be phase shift between them. But as I understand, the phase shift between them should be fixed. In my case, if I fix one A-phase current in the osciliscope, the other one is drifting.
Is someone having the same experience? What I did in the algorithm is only an open loop. I'm using SVPWM, Ud and Uq are fixed value. Switching frequency is 10 kHz, fundamental frequency is 50 Hz.
Thank you in advance for your kind help.