This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Whether users could write the memory space in the Peripheral Frames which is not occupied by registers?



Dear engineers,

                       Thanks for your time! I note that in 28335, some space in Peripheral Frames are not occupied by registers. For example, in Peripheral Frame 3, the McBSP-B registers occupied the memory from the address 0x5040--0x507F, while ePWM1 registers occupied the memory from the address 0x5800--0x583F.  And no registers are on the address 0x5080--0x57FF. So can we use this section for other purposes?

                 Thanks a lot!

                                                                                                                                                Tony Chopper