Other Parts Discussed in Thread: DRV8301, INSTASPIN-BLDC, DRV8312, MOTORWARE
Hi,
I will try to describe my problem,
I'm working with the drv8301 -HC-C2-KIT and runnig a U8 motor that can reach up to speed of 3000 RPM.
For some reason i can't rotate the motor faster than 1000 rpm with the instaspin gui.
Iv'e tried changing the speed with all of the control methods. The motor exerts the right voltage and current by the U8 spec sheet and yet it does not pass 1000 rpm no matter how much current or voltage it exerts.
Are there additional things u know of the we can try to fix the problem?
Thanks!!