Other Parts Discussed in Thread: TMS320F28335, ISO1050
HI
I am working with CAN on TMS320F28335 and using CAN transceiver ISO1050 EVM texas board.I can establish a successful CAN communication. But there are certain issues with the EVM.
I might be worng,but this is my analysis:
A. ISO1050 EVM = Texas board(with 60 ohm terminating resistor and 49.9 ohm resistor between TXD and GND1)
B. ISO1050 EVM = self made board, similar to TI EVM board but without 60 ohm terminating resistor
C. ISO1050 EVM = self made board,similar to TI EVM board but with 60 ohm terminating resistor and no 49.9 ohm resistor in between TXD and GND1.
My setup looks like this:
I need to communicate between DSP1 and DSP2 using CAN (bidirectionally,as CAN is bidirectional).
Now When I use EVM board A - B,transmission happens in direction A to B but not in B to A.
but when i use board B - C,transmission happens bidirectionally and successful CAN communication and data is sent.
I do understand why terminating resistor is required and why it has to be removed from one of the board.But why isn't the transmission happening in direction B to A...Why successful communication takes plave only when 50 ohm resistor between TXD and GND1 is removed from board C.
Is there any significance of this resistor? If I am wrong then how to establish communication with TI board A and board B.Please clarify my doubts.
Thanks & Regards
Sneha