I am using timer interrupt on 28062 processor.
First time i configure the timer to 5 ms using Configcputimer function.
I get interrupt at 5ms everytime.
But i want to modify the period once the interrupt comes.
but no matter what i am unable to do so.
I have written to Cputimer0.periodinus and the value stays there.
then i set TRB bit.
and tried other things to get 1 ms interrupt. No matter what the interrupt will only come at 5 ms.
i tried stopping starting timer using TSS etc....but all is waste.
i also tried this
CpuTimer0Regs.TCR.all = 0x4001;
calling the config function in the interrupt hangs the processor and no code runs.
If i am unable to change the period easily and on the fly its really pathetic on the part of the processor. I wonder how are these processors even being sold.
and i am no newbie.