Hello everyone,
I know that the TMDSPLCKIT-V3 operated in 230 AC environment and also in DC. Although I do not exactly how big can be this DC voltage. Nevertheless I suspect it cannot be high (above 40 V). If it were intended to connect the TMDSPLCKIT-V3 to a link with higher DC voltages (400 V - 700 V), which special considerations must be have into account?
Thanks in advance.
Diego Ballen Cantor