This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Devolopment control motor kit and instanSPIN

Hi ,

I have read the web page of DRV8301-HC-C2-KIT . I have to drive a 3-phase BLDC motor of power 500W

I need to understand if with this kit ,can i identify parameters of my motor BLDC ?

With IstanSPIN BLDC , can i drive my motor without  know the value of the parameters ?

What is the most suitable kit DRV8301-HC-C2-KIT or DRV8301-69M-kit ( Ii has istanSPIN FOC ) ?

Best Regards,

Dario Detomaso

  • This kit will drive 15-60V and up to 40A (with the FOC software) or 60A (with the BLDC software).
    It is the most suitable inverter board for you if you have a <60V 500W motor

    I highly recommend ordering the -69M version so that you can use IS-FOC or IS-MOTION. They are superior in performance and ease of use vs. IS-BLDC.