This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28035 - Watchdog reset

Other Parts Discussed in Thread: CONTROLSUITE

Hi,

I need my hardware to go in to soft reset by using watchdog reset, below is the code wirtten to peform reset

 

Testing on C2000 kit with F28035 controcard connected 

***********************************************************************************************

EALLOW;

SysCtrlRegs.

SCSR |= 0x01; //WDOVERRIDE is set 1 to make WDDIS enable

SysCtrlRegs.

SCSR &= 0xFFFD; //WDENINT is set 0 to make WDRST(reset) enable and interrupt disable

SysCtrlRegs.

WDCR |= 0x20; //WDDIS set 0 to Enable Watchdog

EDIS;

EALLOW;

SysCtrlRegs.

WDCR = 0x0094;

EDIS;

************************************************************************************************

With the above code on watchdog reset the system hangs mentioning No source code available at 0x3FF599

I have tried even these even flashing the code on standalone(removing the debugger) then also on restart it doesnt come back to application.

It stays in 0x3FF599, The same code as been working fine for 28335

Please help me on these

 

Thanks

Girish