This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

when i try to connect to a "F28335" an error appear in code composer studio

Other Parts Discussed in Thread: TMS320F28335

hello
when i try to connect to a "F28335" an error appear in code composer studio
that says:

Error connecting to the target:
Error 0x80000240/-604
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.

SC_ERR_LIB_ANY_LOAD <-604>
A required dynamic library could not be installed.
The attempt to load or install the library failed

I am using CCS 3.3  and eZdsp TMS320F28335 board.

what should i do?
would some body please help me?


Regards

Sibin