Hi,
Since my internal RAM is not sufficient to fit my .text file, so i thought of using external memory on chip RAM, Zone 6. I unsure the procedure to initialize the Zone 6.
1) If i using Zone 6, i shall choose "boot to HO"?
2) Do i need to use the ramfuncs user defined section to store functions that will be copied from external RAM into internal RAM?
3) is it a must to add either non bios.cmd or bios.cmd into any project?