Hi to everyone!
After buying the evaluation board, I've made my own Three Phase BLDC Motor Kit with DRV8312 and F28069M, following schematics and removing switches and unnecessary - for me - connectors to save space. I can program with the FTDI the MCU and also interact with him. But, when I try to run the lab 2b of instaspin labs, to identify the motor parameters, a problem appears. The identification cannot complete. The Rs identification phase seems to be ok, and the motor spins, but when the Rated Flux and Ls identification phase starts, the motor stops and starts vibrating. Does anybody know if there are some parameters of user.h - e.g. offset voltages and currents ... - that could affect to my PCB? Any idea will be great! I don't know what to do!
Thanks in Advance,