Other Parts Discussed in Thread: CONTROLSUITE
Hello, I'm using delfino dual
and "sd_card_cpu01" V100 from CONTROLSUITE.
In the file "mmc-F2837x.c"
at row 811 there is "disk_timerproc" routine
which "[...] must be called in period of 10ms [...]"
so in the outer code you have to implement periodic isr.
If I analyze the code I see that this routine decrement two timer ("Timer1" and "Timer2") used
to implement timeouts.
Why not use, for example 64-bit "IPC Counter Register" which is gifted ?