This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LaunchXL-F28027 vs the F28027F

Other Parts Discussed in Thread: LAUNCHXL-F28027F, BOOSTXL-DRV8301, LAUNCHXL-F28069M

Howdy Everybody,

I bought a F28027 not the F, with a BLDC motor control board.  Now that I am getting closer to figuring it out, I noticed that I may have the wrong board as when I originally looked into it the BLDC board said any LaunchXL.

My project that I want to do is a mechanical cutting cow.  (basically a stuffed cow on a rope and pulley system) It just goes back and forth down the fence at varying speeds not real sophisticated.  Will the non F code LaunchXL still do the trick or should I order a F code? 

My end goal is to have a bluetooth remote or make a android app to control it.  Either run a pre programmed file or remotely control it from as far away as 300'

This is essentially what it is  

Thanks for the help!!

  • well, this is a first :) but the application seems really straight forward.

    you need the "F" version to take advantage of the InstaSPIN-FOC solution as some of the library is in on-chip memory of the "F" devices.

    more importantly you need to understand what motor you are trying to control (3-ph BLDC hopefully; what voltage and current?) to first choose the proper inverter hardware. The LAUNCHXL-F28027F and all the software is mean to work with the 24V/10A BOOSTXL-DRV8301. You can certainly wire it up to another inverter, but if one of our others already fits your needs I'd just start with one of those.
    http://www.ti.com/ww/en/mcu/instaspin/tools_software.shtml
  • I am using the BOOSTXL-DRV8301, I have a 24VDC 3 phase brushless DC 8 amp max motor. I guess I just missed the part where the F code was the proper one, I guess I will need to order a F code. I looked over the InstaSPIN and it seems to make the project much simpler. Ill have an extra LAUNCHXL then!
  • uh, yeah, it makes it MUCH easier than trying to write your own motor control software.
    This motor is perfect for the LP+BP combination.

    Another option is the LAUNCHXL-F28069M that we just released today. Will accept the same BOOSTXL-DRV8301 and supports InstaSPIN-FOC and InstaSPIN-MOTION. Plus - it will allow you to plug in a different BoosterPack if you wanted to try integrating more functionality onto the Piccolo MCU.
  • Thanks Chris!!

    I will get one ordered up, must be the new at Mouser as they have it listed for $35, I will just order one direct from TI.  To bad they don't have a store up there as I was in Allen this weekend and drove right by.  Yeah the less code I have to write the better as it still kicks my butt about everytime.  I have a lot of learning to still do. 

    Jake