This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 FLASH boot problem

I am using ezdsp 28335 eval kit.

I need to flash boot the device. I treid execuing the flash example code .The code is loaded into the device with no issues. but after few seconds a s/w break point occurs.

now next time i cut off the power and keep the boot setting in flash mode the code does not execute. Also the frequency test isnt working.

I need to flash the device so that i need not program it everytime it powers up.

Once the code is loaded by flash programmer the device should execute the code on power up.