I am trying to time the following code
GpioDataRegs.GPACLEAR.bit.GPIO31 = 1;
for (i=0; i<25; i++)
{
xdata *= 1.001;
}
GpioDataRegs.GPASET.bit.GPIO31 = 1;
It seems to take over 20 usec on a F28335 controlCARD (which is ridiculous). Even though I believe I have hardware floating point selected in the compiler it still seems to be calling fs_mpy28() which looks like a software implementation. For my project, to get it to compile I have to select Generic C28xx Device. If I select Experimenter's Kit Defino F28335 or just F28335 I get all kinds of memory map errors.