Other Parts Discussed in Thread: DRV8301
Im trying to use my BLDC 48v to run small car that i have build it.
I have done with all labs until 3 and i did inertia id lab also and everything was perfect.
But, when i fixed the motor on my car it wont run it, but when i lift the car and free the tyre, the tyre is rotating as normal an i can control it easily, but when i leave the car on the ground it wont run,!!!!
Is there any other parameters that i have to add it to user.h to make the car run?
Is the problem with the weight ?
When i connect the motor with the controller comes with the motor it runs my car perfectly but i want to use my drv8301 f28069m .
Thanks a lot ,,,