Other Parts Discussed in Thread: TMS320F28PLC83, TMS320F28069, AFE031
Hi,
My requiremenst are still a little fuzzy but here is what I know
Street light control with power line communication. (Controller to be in the light pole base)
125 degrees C (heat dissipation will be an issue).
Lights are broken up on the 3 phases, 230Vac COMMON neutral. (yea I know Common neutral is not code in the USA)
Approximatley 70,000 lights to be controlled.
I don’t know the distances yet….
I'm not sure which standard yet I will have to follow, G3, Prime, or our prime lite.
I'm currently looking at the TMS320F28PLC83 as well as the TMS320F28069 and the AFE031
( I need to run at 125C)
Given that I have 70,000 nodes is there a particular standard you would recommend? how easy/practical is it to have 70,000 unique addressable nodes?
Cheers
Calum