Hi, I was hoping for some help before purchasing a sensor/gps for my board. I have a C200 LaunchXL-F28027 board.
The project is for a semi-Autonomous Sailing boat. I need GPS, wind direction, wind speed, and compass heading. A Airmar sensor can provide all of those by Serial communication, however it is cheaper if i get the Airmar wx models which do everything except the GPS and purchase a GPS separately.
The Airmar unit communicates by RS232 protocol and NMEA string format. I think the GPS will also use NMEA format but is not selected yet.
As a new programmer (almost no experience) will it be easy enough to read from a GPS and a Airmar independently on the same board and use information from both to constantly control a set of motors to turn the boat in the right direction?
Any help or advice would be appreciated.