Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I'm using the Concerto F28M36P63 Controller ( http://www.ti.com/tool/tmdscncd28m36 ).
The DSP is running with 150MHz ( 6,67ns /step).
For an application I want to configure one PWM module (e.g. ePWM1 with high resolution) to work with 16-Bit Resolution.
In normal ePWM mode that leads to a frequency of about 2,288 kHz.
-> ( 150Mhz / 65536 ) = 2,288kHz ( 65536 = 16-Bit Resolution for the PWM timer -> TBPRD Register )
The frequency should be higher for the needed application. ( best would be 100kHz)
In the manual it says that in high Resolution mode (pwmHR) a step size of about 150ps is possible.
With 150ps it should be possible to reach 16-Bit resolution @ 100kHz but I'm not sure how to configure the Registers.
So I've got two questions:
1. Is it possible with the 16-Bit resolution and the 100kHz ( I think it is) ?
2. How do I have to configure the registers?
-> I don't see a possiblity to run the PWM timer with 150ps, only with SYSCLKOUT = 6,67ns
-> Is it enough to configure the compare Register (CMPA / CMPB) in high resolution?
My thought is that the timer must also have high resolution to match the CMPA / CMPB value.
Thanks very much for your answers !!!
Regards
Jens