Hi everyone
On the Code Composer V3.3 for the TMS28335 it is easy to visualize variables using buffers and it is very useful for debugging. I have been not able to do this in the Code Composer V 6.0 for the Concerto, F28M36. It seems that the refresh rate of the graphic window of the Code Composer V 6.0 is not fast enough to capture the dynamics of a 10kHz sampled variable. Is this a limitation of the Code Composer V 6.0 or am I missing something?