I'm having this problem in lab5a where the motor is not accelerating smoothly when applying some/high/max torque. You can see/hear it in this video. When I apply a small enough torque the motor is accelerating smoothly.
It seems like the software is expecting the motor to go faster than it actually does, and ends up with setting too high frequency. I have tried a lot of changes, but nothing gave any useable results.
Calculated Ki(PU): 0.02338
Calculated Kp(PU): 0.8544
Using speedref works great, but torquecontroll is wanted.
Can this have something to do with forcing angle, which is enabled with default values?