Other Parts Discussed in Thread: TMS320F28335, TMS320F2812
Has anyone seen Flash API Error #31 with the following description?
There was a zero bit error on the Program Operation.
First Fail Address = 0x00338645
Expected Data = 0x0ec8
Actual Data = 0x0ec6
The device I am programming is the TMS320F28335.
Coded Composer 3.3.82.13
Code generation tools 5.2.2
Once this condition is set, it is very difficult to clear. The only reliable method I have found to clear it is to reprogram the flash with SDFlash.
I have experienced this problem with both the DSK and target board.