Other Parts Discussed in Thread: TMS320F28335
Hi,
I am facing a problem with TMS320f28335 Internal ADC interfacing. When we are injecting AC signal (Voltage) on pin 47 then the value of ADC output (ac current , injected on pin 48) is increasing up to 2%.
Input Voltage (pin 47): 2.6Vpp
Input current (pin 48) : 0.2789 Vpp
Case-1:
Input current (pin 48) : 0.2789 Vpp
And then with Input Voltage (pin 47): 2.6Vpp ,read value of ADC output at pin 48
Case-2:
Input current (pin 48) : 0.2789 Vpp
And without any Input Voltage (pin 47): 0V , read value of ADC output at pin 48
In both cases , output is varying up to 2%.
Please suggest me any solution.