The "labs" indicate that for low inductance motors I need to increase the PWM frequencies. But how do I know that my motor is "low inductance"?
I'm currently running a motor that is detected as 115uH. It has 68 mOhm Rs. Is this low?
Apparently the cogging force on my motors are "high", this causes the motor not to spin during the tests (with the default configuration). As normal sensorless drivers manage to spin this type of motor, and work from the back-emf once it is spinning fast enough, shoudn't the estimator "verify" that it is spinning by using the back-emf? Now it just gets "bad results".