This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Warning: #10083-D LOAD placement ignored for "RamParameterDataObject": object is uninitialized



Hi All,

I am using TMS30F2812 MCU.

I am running my application from flash memory. However, 2 variables are copied in RAM.

For copying variables in RAM, i have written following code:

In Main.c

#pragma DATA_SECTION(tTMS320F2812ECanaTransactionParameterDataObject, "RamParameterDataObject")
volatile t__TMS320F2812ECanaTransactionParameterDataObject tTMS320F2812ECanaTransactionParameterDataObject;

#pragma DATA_SECTION(tTMS320F2812ECanaTransactionStatusFlags, "RamTransactionStatusFlags")
volatile t__TMS320F2812ECanaTransactionStatusFlags tTMS320F2812ECanaTransactionStatusFlags;

/* Initialize the RamParameterDataObject section */
memcpy(&u16RamParameterDataObject_RunStart, &u16RamParameterDataObject_LoadStart, (Uint32)&u16RamParameterDataObject_LoadSize);

/* Initialize the RamTransactionStatusFlags section */
memcpy(&u16RamTransactionStatusFlags_RunStart, &u16RamTransactionStatusFlags_LoadStart, (Uint32)&u16RamTransactionStatusFlags_LoadSize);

In Main.h

extern Uint16 u16RamParameterDataObject_LoadStart;
extern Uint16 u16RamParameterDataObject_LoadSize;
extern Uint16 u16RamParameterDataObject_RunStart;


extern Uint16 u16RamTransactionStatusFlags_LoadStart;
extern Uint16 u16RamTransactionStatusFlags_LoadSize;
extern Uint16 u16RamTransactionStatusFlags_RunStart;


In F2812.cmd

    /*** User Defined Sections ***/
    RamParameterDataObject: LOAD = FLASHC, PAGE = 0
                            RUN = RAMM0,   PAGE = 1
                            LOAD_START(_u16RamParameterDataObject_LoadStart),
                            LOAD_SIZE(_u16RamParameterDataObject_LoadSize),
                            RUN_START(_u16RamParameterDataObject_RunStart)

    RamTransactionStatusFlags: LOAD = FLASHC, PAGE = 0
                               RUN = RAMM0,   PAGE = 1
                               LOAD_START(_u16RamTransactionStatusFlags_LoadStart),
                               LOAD_SIZE(_u16RamTransactionStatusFlags_LoadSize),
                               RUN_START(_u16RamTransactionStatusFlags_RunStart)

I have followed the procedure mentioned in application note SPRA958L.pdf. Section 4.6.2, page 19 and page 20.

Still i am getting following warnings:

#10083-D LOAD placement ignored for "RamParameterDataObject":  object is uninitialized

#10083-D LOAD placement ignored for "RamTransactionStatusFlags":  object is uninitialized

Please suggest way to suppress the warning.

Thank you,

Sunil Sawant

  • Hi Sunil,

    Please refer this doc for copying sections from Flash to RAM while execution:

    Flash to RAM.pdf

    Regards,

    Gautam

  • Sunil,

    RamParameterDataObject and RamTransactionStatusFlags are uninitialized variables. That is, they have no initial value. There is nothing to copy. They should just be linked to RAM, not flash. It's like doing this:

    int x;

    'x' is a variable. It has no value until you give it one in the code. Therefore, there is nothing to copy. You cannot link x to flash. It should be linked to RAM, and again there is nothing to copy.

    Regards,
    David