This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Internal Error in Code Composer Studio 3.3

Hello,

I have 2 computers with an older version of code composer (CCS 3.3) that I use to compile code for a F28335.

Yesterday I found that something happened with the compiler tools.

I'm getting a "INTERNAL ERROR" regarding the asm2000.exe tool when assembling.

I've tryied older code version (that always worked) and I'm getting the same error.

Is anyone getting the same problem?

I had a problem with the Panda Antivirus and got an update from Windows in my Windows 7 yesterday, maybe this is connected.

"INTERNAL ERROR:

C:\Program Files (x86)\Texas Instruments\C2000 Code Generation Tools 5.0.1\bin\asm2000.exe

experienced a segmentation fault while
processing section .text file C:\Users\1033\AppData\Local\Temp\0994031 line 7173"

Best regards, Jorge Lopes