This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN communication between two different Micro controller

Dear Sir,

Is it possible to setup communication between C28069 and F28M35H52C1.?

I have two different board. One is using F28M35H52C1 concerto device and another is using C28069. I have do not have spare Serial communication port in any of the board and also i need to use high sepeed communication.

So please any one can tell me that can is possible or not in between these two ?

Umang 

  • Umang,

    Assuming both boards have a CAN transceiver and a way to connect them, then yes the CANs on each can communicate.

    Regards
    Lori
  • Umang,

                Not sure I understand your question well. Sure, you can have the CAN module in these two devices communicate with each other. That is the objective of these modules. CAN is an industry-standard protocol and you can connect multiple devices (even from different manufacturers) to the bus. I am assuming you have CAN transceivers on-board. You cannot directly connect the CAN pins together. Let me know if I addressed your concerns.