Other Parts Discussed in Thread: TMS320F28027, CONTROLSUITE
Hi, I am using the C2000 LaunchPad (TMS320F28027) for communication purposes using SPI and SCI ports.
I have successfully compiled the examples from controlSUITE (controlSUITE\device_support\f2802x\v129\DSP2802x_examples_ccsv4) using CCSv6, and have also debugged them loading the code into the RAM.
The examples that I am trying are sci_echoback and spi_loopback, which I have modified in order to send data to an Arduino Uno board. The problem that I ma facing is that the data that the Arduino receives is always the same, although is change over time.
I have already checked all the register of TMS320F28027 and they seem to be fine.
Any suggestion in order to solve this problem?
Thanks in advance for any help you could provide.
Best regards,
Gus.