This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 PLC Dev. Kit (TMDSPLCKIT-V3)

So I am just messing around with the GUI included in this development kit.  I can get the modems to work on one PC, but I cannot get them to work on two separate PC's running two separate GUI's.  Is this something that is even possible?  I am running version 2.103 of the Zero Config. GUI.  Thanks so much for your help.  

  • Hi Aaron,

    You should very well be able able to run the same kit on 2 different PCs. Does the kit get recognized in the other PC?

    Regards,
    Gautam
  • I'm sorry, my wording was poor. I meant that I cannot get the modems to communicate while connected on two separate PC's. One modem connected to computer A and one to computer B. Is this connection possible? ComputerA/Modem A/GUI-A <-----> ComputerB/ModemB/GUI-B.
  • Aaron,

    Yes, this is possible. 

    You've said that you can run the 2 GUIs on one PC and have everything work.  Have you tried doing this on both computers separately?

    My guess is that (a) one of your computers has some type of driver issue or (b) one of the computers has an old version of the Zero Configuration GUI installed.


    Thank you,
    Brett