Other Parts Discussed in Thread: CONTROLSUITE
HOW TO MAKE A PROJECT FILE IN CCSV6 FOR EXPERIMENTAL KIT F28027..??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
HOW TO MAKE A PROJECT FILE IN CCSV6 FOR EXPERIMENTAL KIT F28027..??
Hi Reyyan,
You can follow this guide to start a project from scratch: 8802.C2000_launchpad_basics.pdf
You can also import sample projects from controlSuite (you need to download this software if you don't have it)
C:\ti\controlSUITE\device_support\f2802x\v129\DSP2802x_examples_ccsv4
Regards,
Gautam
Hi Reyyan,
I think you should install the driver for XDS emulator.
Regards,
Phien Nguyen Thanh
http://www.digikey.com/product-detail/en/TMDSDOCK28027/296-31062-ND/2696320
this is link.. but i am sure about it is experimenter's kit (docking station + control Card)
i am working on an other project having error
**** Build of configuration F2802x_FLASH for project FlashingLeds-F28027 ****
"c:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building target: FlashingLeds.out'
'Invoking: C2000 Linker'
"c:/ti/ccsv6/tools/compiler/c2000_6.2.5/bin/cl2000" -v28 -ml -mt -g --define="_DEBUG" --define="LARGE_MODEL" --define="FLASH" --diag_warning=225 -z -m"FlashingLeds.map" --stack_size=0x380 --warn_sections -i"c:/ti/ccsv6/tools/compiler/c2000_6.2.5/lib" -i"c:/ti/ccsv6/tools/compiler/c2000_6.2.5/include" -i"C:/Users/Ali Muhammad/workspace_v6_0/exercise/FlashingLeds-F28027" --reread_libs --xml_link_info="FlashingLeds_linkInfo.xml" --rom_model -o "FlashingLeds.out" "./SciCommsGui.obj" "./FlashingLeds-Main.obj" "./FlashingLeds-DevInit_F2802x.obj" "./Example_2802xFlash.obj" "./DSP2802x_GlobalVariableDefs.obj" "./DSP2802x_CodeStartBranch.obj" "C:/ti/controlSUITE/device_support/f2802x/v129/DSP2802x_common/cmd/28027_RAM_lnk.cmd" "C:/ti/controlSUITE/device_support/f2802x/v127/DSP2802x_headers/cmd/DSP2802x_Headers_nonBIOS.cmd" "../F28027_FLASH_FlashingLeds.CMD" -l"libc.a"
<Linking>
"../F28027_FLASH_FlashingLeds.CMD", line 51: error: BOOT_RSVD memory range
overlaps existing memory range BEGIN
"../F28027_FLASH_FlashingLeds.CMD", line 52: error: progRAM memory range
overlaps existing memory range PRAML0
"../F28027_FLASH_FlashingLeds.CMD", line 59: error: BEGIN memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 62: error: IQTABLES memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 62: error: IQTABLES memory range
overlaps existing memory range IQTABLES
"../F28027_FLASH_FlashingLeds.CMD", line 63: error: IQTABLES2 memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 63: error: IQTABLES2 memory range
overlaps existing memory range IQTABLES2
"../F28027_FLASH_FlashingLeds.CMD", line 64: error: IQTABLES3 memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 64: error: IQTABLES3 memory range
overlaps existing memory range IQTABLES3
"../F28027_FLASH_FlashingLeds.CMD", line 66: error: BOOTROM memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 66: error: BOOTROM memory range
overlaps existing memory range BOOTROM
"../F28027_FLASH_FlashingLeds.CMD", line 67: error: RESET memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 67: error: RESET memory range overlaps
existing memory range RESET
"../F28027_FLASH_FlashingLeds.CMD", line 77: error: RAMM1 memory range has
already been specified
"../F28027_FLASH_FlashingLeds.CMD", line 77: error: RAMM1 memory range overlaps
existing memory range RAMM1
"../F28027_FLASH_FlashingLeds.CMD", line 78: error: dataRAM memory range
overlaps existing memory range DRAML0
error: symbol "_main" redefined: first defined in "./FlashingLeds-Main.obj";
redefined in "./Example_2802xFlash.obj"
error: errors encountered during linking; "FlashingLeds.out" not built
>> Compilation failure
gmake: *** [FlashingLeds.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
i successfully build by project and it is working.. kindly u send me all lab session so that i have better information about how this device can work and thank for giving me suggestion