This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi:
I am working with F28M35H52C1 Concerto Card . I can not excaute enet_uip applied by controlsuite version lower than 3.3.1 which halt the second while in ethernet.c .
as follow :
void EthernetPHYWrite(unsigned long ulBase, unsigned char ucRegAddr,unsigned long ulData)
{
// Check the arguments.
ASSERT(ulBase == ETH_BASE);
// Wait for any pending transaction to complete.
while(HWREG(ulBase + MAC_O_MCTL) & MAC_MCTL_START)
{
}
// Program the DATA to be written.
HWREG(ulBase + MAC_O_MTXD) = ulData & MAC_MTXD_MDTX_M;
// Program the PHY register address and initiate the transaction.
HWREG(ulBase + MAC_O_MCTL) = (((ucRegAddr << 3) & MAC_MCTL_REGADR_M) |
MAC_MCTL_WRITE | MAC_MCTL_START);
// Wait for the write transaction to complete.
while(HWREG(ulBase + MAC_O_MCTL) & MAC_MCTL_START)
{
}
}
I am sure the hardware setting is correct.
So,what i can do ?
What revision Silicon are you using ?
Thanks
Noah