Hello,
At the moment, without any changes made to the HW, I am getting the same performance level from InstaSPIN as my other ESC. I followed the lab guides, and have done multiple tests but I don't notice any major differences in efficiency at all. [I used a Watt meter to calculate the input power, and I calculated the thrust generated from the rotor blades to work out the output power.] I read that many users found success in boosting overall efficiency by ~20% using InstaSPIN. The only step I haven't taken yet is HW optimisation, and I assume this is necessary in order to see the same result as the others.
I have been reading the Spruhj1f document, and I see Section 5.2.3-5.2.5 give examples on the calculation procedures. I'm currently using BOOSTXL-DRV8301, am I right to assume that I should follow the same procedure as well? What resistors and capacitors do I need to change? I'm confused by the schematic of DRV8301 Boosterpack's "Phase C Current Sense" diagram, because I see two amplifiers there and I'm not quite sure how to approach the "U3B" part.
a) For the Current Feedback Gain, I attempted "U3A" and I had R43 and R47 as the Rfbk, R44 and R45 as Rin (1.00k Ohm), and R34 as the shunt resistor (0.01k Ohm).
Iin is 15A:
(3.3 - 1.65) / (15 x 0.01) = 11
Rfbk = 11 x Rin = 11k Ohm with Rin = 1k Ohm
So I should change R43 and R47 to 11k Ohm resistors, am I right? (R43 and R47 are currently 10k Ohm)
b) For Voltage Feedback,
Vamax is 19.5V (15V + 30% headroom)
19.5 = 3.3 x (4.99k + Rvu) / 4.99k
Rvu = 24.5k Ohm
So I need to replace R37, R39 and R41 with 24.5k Ohm resistors, am I also right? (R37, R39 and R41 are currently 34.8k Ohm)
c) Filter pole... pardon my newbie question but what is "filter pole" exactly?
C34, C35 and C36 are 0.1e-6 F
Ffilter_pole = 1 / [2 x Pi x 0.1e-6 x (24.5k x 4.99k / 24.5k + 4.99k)] = 383.91 Hz
But from the DRV8301 EVM HW guide, there seems to be a different approach:
- My motor has 7 pole pairs; 9 kRPM
- Hz = RPM x Poles / 120 = 9000 x 14 / 120 = 1050 Hz
- Select 1100 Hz (>1050 Hz)
- Rvu = 24.5k Ohm and Rvl = 4.99k Ohm
Ffilter_pole = 1100 Hz = 1 / [2 x Pi x (24.5k x 4.99k / 24.5k + 4.99k) x C]
C = 34.9 nF
So am I supposed to change the capacitors? If so, are my calculations correct?
Thanks,
Yau