This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C2000] Code built with codegen 5.0.0B2 doesn't build with 5.2.2

Hello,

 

 I have the same problem: with c2000 v5.0.0B2 I was able to build properly, but with 5.2.2 not any more. The update advisor tell me, my system is up-to-date. More over, I'm unable to downgrade to 5.0.2.  Is there any solution?

 

Tanks

  • Mester said:
    I have the same problem: with c2000 v5.0.0B2 I was able to build properly, but with 5.2.2 not any more. The update advisor tell me, my system is up-to-date. More over, I'm unable to downgrade to 5.0.2.  Is there any solution?

    For CCS 3.3 there should be an up date for codegen 5.2.5 on update advisor under codegen tools.  First please update to that release

    If there are still problems, then please post more more information on the failure in the C/C++ Compiler Forum.

    • Which device you are building for
    • Tools version number
    • Reproducible test case as attachment
      • Only needs to build to object, does not need to link and run
      • If you cannot attach a file to the post directly, try adding a file to the Files tab in your user profile
      • Access your profile by clicking on your name in the forum
    • Use this technique to avoid the pain of sending all those header files
    • The exact build options

    http://tiexpressdsp.com/index.php/Before_asking_for_CGT_support

    Regards

    Lori