All:
It definitely appears that the F28075 part is a great part!
A few questions:
1. When enabling flash pipelining, does the flash run at the effective 120 MIPs speed (similar to F28069)?
2. There are some places that state it is a single 3.3 volt part, but others that say that 3.3v and 1.2v are needed (because internal voltage regulator was not yet working?)
3. I have seen one 1K unit pricing as low as $8.41 (28074) and another place where it is ~$10. Which is correct?
4. It definitely looks like one can migrate from an existing F28335 design to the F2807x with minimal problems...
a. External oscillator (30 MHz) may not be needed if internal can be used. Is CAN the only situation where an external oscillator is required?
b. Obviously there are changes in ADC12, but it looks like the F2807x may have a "better" ADC than previous parts?
c. Are there any other major changes to be aware of? (For instance, EMIF?, Comm changes?)
5. When do you expect volume production? (Is the F28075 at TMS or TMX or does that even make sense anymore?)