Hi all
I’ve some problems with F28M35H52C1 Rev B.
I designed a board with F28M35-Rev0, that well programmed by XDS100 V2
But new boards with F28M35H52C1 Rev B have some bugs. When I want to program the chip by, CCS 5.3.0, I find the warning that “Device ID is not recognized or is not supported by driver”.
By the way; Programing the RAM of the chip by Debugger, shows other problems. For example a sample program in Control Suite “Timer Sample for DSP core” that blinks LED every 1 sec with CPU Timer. It works very well with F28M35-Rev0. But the board with F28M35H52C1 Rev B blinks every 15 seconds.
Can anyone Help?